AXIS#.SETTLE.V

Description

Within AXIS#.MOTIONSTAT, AXIS#.SETTLE.V is used to indicate that the target velocity of a motion task has been reached. AXIS#.MOTIONSTAT displays a "Target Velocity Reached" bit as soon as the following statement becomes true:

(target velocity – AXIS#.SETTLE.V) < AXIS.VL.FBFILTER < (target velocity + AXIS#.SETTLE.V)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Depends on AXIS#.UNIT.VROTARY

Rotary: rpm, rps, deg/s, Custom Units/s, rad/s

Range

Rotary:

0.000 to 15,000.000 rpm

0.000 to 250.000 rps

0.000 to 90,000.000 deg/s

0.000 to 1,250.000 Custom Units/s

0.000 to 1,570.796 rad/s

Default Value

Rotary:

60.000 rpm

1.000 rps

359.999 deg/s

5.000 Custom Units/s

6.283 rad/s

Data Type

Float

See Also

AXIS#.MOTIONSTAT

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SETTLE.V

5016h

02h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7101

1

7101 (0x1bbd)

AXIS1.SETTLE.V

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.SETTLE.V

7101

Float

Read/Write

Velocity